Perhaps it's all due to the 33MHz crystal circuit...
Can someone please tell me what voltage level I should see? I have a board derived from the DM6467T EVM, and when I put a scope on the crystal side closest to DM6467T pin "DEV_MX0", I see a 33MHz signal but it only varies from 0.32V to 1.68V (1.36V p-p). This is a TMS320DM6467ZUTD1 with core power supply 1.244V (plus 1.8V and 3.3V elsewhere).
On a different build of the same board, I have a TMS320DM6467ZUT7 with a 27MHz crystal, 1.199V power supply (plus 1.8V and 3.3V elsewhere). On this board, the same side of the crystal (but the 27MHz instead of 33MHz crystal), the side near "DEV_MX0", I read a 27MHz signal that varies from -0.96V to 2.92V (3.88V p-p).
I don't think the weaker 33MHz signal is due to my 60MHz Techtronix TDS 210 Digital Scope. But then I don't know if the weaker signal is right or wrong!
Note, the TMS320DM6467TZUTD1 chip was hot as heck just now when I switched back to the TMS320DM6467ZUT7 board.
ANYWAY, in trying to flash nand on the board, the furthest I get connecting with the XDS510USB using CCS4 (WinXP/VMWare) is to where I load the target program "nand_flash_writer.out". I get an error "Data verification failed at address 0x8802B134 Please verify target memory and memory map." This *is* a fresh board, and the fab house is known to have difficulty with BGA's, of which all three DaVinci, dual DDR2 chips, and NAND chip are BGA's. I don't know if this error is due to an actual DDR2 error, or because the DaVinci is not running fully due to the weak crystal signal. Note that I can indeed load "nand_flash_writer.out" when my XDS510USB is connected to the older board, the one with the ...ZUT7.
Note that prior to the load target program step, when I try to load the target configuration and then connect to the target, the connect to target step often never completes. I hit this first, which is why I thought I might have crystal problems. I reflowed the solder on some sand grains (size 0402 resistor and caps), to go from sometimes seeing the 33MHz signal on the scope to always seeing it. (Yes, scoping crystal signals is always iffy.)
Occam's Razor? Am I having just one problem? If so, the crystal seems more suspect, wouldn't you think? I would think the trouble connecting to the target at all should have nothing to do with DDR2. But it might have to do with the DaVinci BGA itself, with poor solder joints and heat. I don't know.
If I'm having two problems, then maybe it's both DaVinci and dual DDR2 BGA's.
The only possibly KNOWN THING, is what kind of voltage levels SHOULD I bee seeing on the 33MHz crystal?
Many thanks for any advice.
-Helmut