This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359: Is it possible to use clockevent timer2 other than timer3(other timer) in kernel?

Part Number: AM3359

HI

Is it possible to use clockevent  timer2  other than timer3(other timer)  in kernel?

For example, can it be used by changing clockevent timer2 => 3 as shown below?

root@am335x-evm:/root# dmesg | grep timer
[ 0.000000] OMAP clockevent source: timer3 at 24000000 Hz
[ 0.000038] clocksource timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000050] OMAP clocksource: timer1 at 24000000 Hz
[ 0.246080] Switched to clocksource timer1
[ 0.260753] omap_timer am33xx-test_module_timer: omap_dm_timer_probe: no IRQ resource.
[ 22.380343] gptimer test: GP Timer initialized and started (24000 Hz, IRQ 166)
root@am335x-evm:/root#

Is it possible to use clockevent  timer2  other than timer3(other timer)  in kernel?

Thank you.