This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM572X: Can I get the DataQ for each output value?

Part Number: TMDSEVM572X

Processor SDK: 06_03_00_106

Hello, TI!

When I run the TIDL layer_output example, it will create "trace*.info" files including DataQ, maxValue and minValue.

Supposing the output is 1*64*64(chanel*height*width),

(1) do the maxValue and minValue in the "info" files mean the maximum and minimum DataQ for the output matrix?  And the "DataQ" term indicates the average value?

(2) can I get the DataQ for each element in the output matrix?

Thanks!