Part Number: TDA4VM
Hi Champs,
looks like gstreamer does not support video encoding yet. When is that planned?
Do we plan to write on OVX-kernel so that video encoding can be used in an OpenVX graph?
Thanks and kind regards,
one and zero
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Hi Champs,
looks like gstreamer does not support video encoding yet. When is that planned?
Do we plan to write on OVX-kernel so that video encoding can be used in an OpenVX graph?
Thanks and kind regards,
one and zero
Hi,
Video encode/decode will be supported as V4L2 driver, so i think it should be possible to either integrate it with the OpenVX application or even have OpenVX node on top of it.
We are still looking into how to integrate V4L2 encode/decode with the OpenVX application.
Regards,
Brijesh
Hi Brijesh,
when will video decode and encode be supported?
When will we know if we plan do write an OpenVX kernel for 4L2 encode/decode?
Kind regards,
one and zero
Hi,
I think encode and decode based on V4L2 are already part of the SDK8.1 release.
Please refer to the roadmap slides for more information.
Regards,
Brijesh
Hi,
Confirmed with the team that gStreamer plugin for encode & decode is supported in sdk8.1 release.
We can check it by running
You can check by running
gst-inspect-1.0 | grep "v4l2"
Rgds,
Brijesh