Hi, Expert,
In J7 , we use VXE384MP2 to encode the video stream. I have below questions .

According to the TRM explanation, the max throughput of the encoder is 3*1080p@30Hz, However, encoder, in general, has its own limitation on max frame resolution. For example, a frame of 15360x135 also has 2M pixels, however, not every 1080p encoders can support such odd resolution.
Can you pls help to share our supported resolution ? Thanks.
In a mix encoding resolution. Is it possible for simultaneously usage of 1280x720/1920x1080 or the 3 channel resolution must be the same?
Regards,
Fredy Zhang