This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6711D: Boot issue

Part Number: TMS320C6711D


Hello,

We are using the C6711D in our product and we meet a rate of 20 to 40% of unsuccesfull starts. 

Our software boot in internal flash on a boot loader witch load the firmware in RAM. The first instruction of our boot is to set at 1 the pin Timer1 TOUT1.

The electrical reset is managed by the device (LTC2901) which asserts a reset with 150ms duration. This device is also an external watchdog refreshed by C6711D pin Timer1 TOUT1.

On unsuccesfull starts :

  • After reset, we have the 7.5MHz on the clock-out pin with CLKIN at 20MHz.
  • Timer1 TOUT1 pin stay at 0.

It seems the boot mode selection is not stable. The issue seems to be hardware issue. Which could be the root causes ?

For information, we added the following pullup and pulldown :

  • HD4 : pulldown 1K
  • HD8 : pullup 1K
  • HD12 : pullup 1K
  • RESET : pullup 1K
  • CLKMODE0 : pullup

Many thanks for your help.