Other Parts Discussed in Thread: TVP5158
Hi !
As we know , there are three kinds of model in the DM6467 family: DM6467(-594MHz), DM6467(-729MHz), DM6467T(1GHz).
Recently, I got some problems with my custom board. After checking my Hardware design, I found that my board uses a 594MHz -DM6467, and the ddr2 controller is connected to a 400MHz DDR2. The DDR2 is K4T1G164QE-HCF7( 64MX16).
Does DM6467(-594) support 400MHz DDR2? If not, would you tell me the best way to modify my design ? Which kind frequency of DDR2 could I use ?
If I want to implement 8-ch D1 capture with 2 tvp5158, is DM6467(-594 ) strong enough ?
Thank you very much .