Hello, we are using tms320c6657 and DP83867 for ethernet circuit design and currently encountered the following problems:
We can access the registers of the PHY chip through MDIO, and can read the feedback value. Both the PHY register and the hardware LINK LED indicate that it links up. However, when reading the DSP SGMII register and the EMAC register, it shows that the link is not successful.
The same code can be debugged using the development board. The following is a comparison of the relevant registers of the development board and our own board.