This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMIC110: AMIC110 McSPI single channel (Master)

Part Number: AMIC110

Hi,

I am using AMIC110 CUSTUM board to  SPI interface with EEPROM . During interfacing my observations are :

1. If I configure SCLK pin as output via disabling the CONF_<module>_<pin>_RXACTIVE bit then I can able to transmit  data properly but I am not able read data into the SPI Buffer.

2. If I configure SCLK pin as input or output via enabling the CONF_<module>_<pin>_RXACTIVE bit then I can able to transmit and receive data properly into the SPI Buffer.

I further like to understand the above interpretation. 

Thanks,

Anil Garg