This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: [C6678] use Two Ethernet port

Part Number: TMS320C6678

Hi, I have a custom board of c6678 with two ethernet ports.

I already use Port 0 on Core 0. ( QMSS + CPPI + PA + NIMU)
And I need to add Port 1 on Core 1.

What should I do?

can i get example code for dual Port/Phy Etherenet?

ps: my ccs version is: 9.3.0
ndk version: 2.25.1.11
pdk version: 2.0.15
bios version: 6.76.2.02