Other Parts Discussed in Thread: CCSTUDIO
I have been trying to get an XDS510USB emulator to work with several versions of CCS. I have tried CCS3.3, 4.2, 5.02 (latest available for download). And have setup and followed several guides on this website however I always get the following error..
Error connecting to the target:
Error 0x80002240/-115
Fatal Error during: Initialization, OCS, Control,
Or some equivalent version of it in the specific version of CCS.
My question is. Should I be able to use this emulator (XDS510USB) with an evaluation licence (or the 90 day extension licence) of CCS XXX, or do I need a real/full licence?
Note: BlackHawk test/check utilities do not find any errors related to the XDS510USB emulator.
Note: I'm trying to connect to an L138 EVM.
Thanks,
- Orlando