I am interested in using the DSP within the OMAP3530 to read and write to a MMC device. There is a note on the bottom of page 188 on the OMAP3530 TRM (spruf98p) which states "IVA2.2 subsystem (DSP) can’t access SoC peripherals". This suggests that the DSP cannot access the MMC. Is this statement correct?
By observation, when JTAG-debugging the DSP I can read/write SOC peripheral memory-mapped registers. Also there is a thread on this forum ("How to access external peripheral from C64x+ DSP") which discusses DSP access to a memory-mapped peripheral (FPGA on CS4 in this case). Is this access somehow different than accessing the MMC?
The short question would be: can I access a device on MMC from the DSP?
Thanks in advance for your comments.
Sam.