Other Parts Discussed in Thread: TVP5150AM1
Hi everyone,
I have some questions about DM365 use TVP5150AM1 to capture video.My system 's hardware and software are describe as below :
I just use AIP1A to capture video.The analog Video signal is from a VCR output .TVP5150AM1 's YOUT[0..7] connect to DM365 's YIN[0..7] and use SCLK as CLK .
The YCbCr output format is 8bit ITU-R BT.656interface with embedded sync.
I capture the video and use UYVY's standard to save them.I don't use any compressd type and save the original signals to a file .Then i use UYVY & YUV player to play the file on my PC, but i found :
1, Compared with the TVP5150AM1 input video source , some frame are lost , Why?
2,The Video display so fast , i use the same player to play other video file and the video source file ,the speed is normal. Why?
3, Same frame cann't display normaly . They contain some harsh color, Why ?
Can anyone help me?
Thanks in advance.