This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: Can device boot from USB when a usb hub is used?

Part Number: AM6442

Hello,

the device only have one USB interface. Therefore we'd like to multiple the port by using a USB hub. 

But we would also like to keep the usb boot feature. Is it possible to use usb boot even when there is a usb hub in between?

BTW: I tried with an external HUB, but it didn't work.

Best,

Artur Töws