This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am trying to build C++ application from j721e but running into build errors. Is there a demo application that shows how to build a C++ application from PDK?
Hi,
You can apply the below patch on the top of SDK 8.1.
0001-C-Demo.patch
Please follow the procedure below to apply the patch:
Patch contains makerules changes to incorporate C++ build and a demo application in form of a diagnostic example.
The patch has been validated on j721e SDK 8.1. The demo application can be built for MCU and MPU core with the following command in <pdkInstallPath>\packages\ti\build
gmake BOARD=j721e_evm CORE=mcu1_0 CPLUSPLUS_BUILD=yes board_diag_cppTest
gmake BOARD=j721e_evm CORE=mpu1_0 CPLUSPLUS_BUILD=yes board_diag_cppTest
Regards,
Parth