Other Parts Discussed in Thread: TMS320C6678, UCD9222, UCD7242
In my design I'm using the UCD9222 with UCD7242 to supply the core voltages of TMS320C6678, as in the DSP EVM.
1.From what I understood, the UCD9222 FLASH can be programmed using the I2C or the JTAG link, please confirm.
2.Can I connect the UCD9222 JTAG on the same JTAG chain, with the TMS320C6678?
3.On the DSP EVM, which device is being used to program the UCD9222 – the FPGA or the DSP (the I2C port is connected to both devices)?
4. Can you provide the initialization data of the UCD9222, as being used in the 6678 DSP EVM (parameters being set, e.g. switching freq, timing, voltages, current limits, etc. as well as the registers settings)?
Regards,
Erez