Hello,
Background:
I have trained model using repository - https://github.com/TexasInstruments/edgeai-yolov5
No modifications are done to network, only custom data is used to train for few epochs.
Pretrained network at https://github.com/TexasInstruments/edgeai-yolov5/tree/master/pretrained_models/models/yolov5s6_640_ti_lite was used.
After exporting to onnx and trying to compile on TDA4VM I get following error:
RuntimeExceptionTraceback (most recent call last) <ipython-input-4-bb2e73c005ce> in <module> 30 so = rt.SessionOptions() 31 EP_list = ['TIDLCompilationProvider','CPUExecutionProvider'] ---> 32 sess = rt.InferenceSession(onnx_model_path ,providers=EP_list, provider_options=[compile_options, {}], sess_options=so) 33 34 input_details = sess.get_inputs() /usr/local/lib/python3.6/dist-packages/onnxruntime/capi/onnxruntime_inference_collection.py in __init__(self, path_or_bytes, sess_options, providers, provider_options) 281 282 try: --> 283 self._create_inference_session(providers, provider_options) 284 except RuntimeError: 285 if self._enable_fallback: /usr/local/lib/python3.6/dist-packages/onnxruntime/capi/onnxruntime_inference_collection.py in _create_inference_session(self, providers, provider_options) 313 314 # initialize the C++ InferenceSession --> 315 sess.initialize_session(providers, provider_options) 316 317 self._sess = sess RuntimeException: [ONNXRuntimeError] : 6 : RUNTIME_EXCEPTION : Exception during initialization: /home/a0133185/ti/GIT_C7x_MMA_TIDL/c7x-mma-tidl/ti_dl/release/build_cloud/test/onnxruntime/onnxruntime/core/providers/tidl/tidl_execution_provider.cc:170 virtual std::vector<std::unique_ptr<onnxruntime::ComputeCapability> > onnxruntime::TidlExecutionProvider::GetCapability(const onnxruntime::GraphViewer&, const std::vector<const onnxruntime::KernelRegistry*>&) const graph_build.Resolve().IsOK() was false.
The compilation option used are as below:
compile_options = {
'tidl_tools_path' : os.environ['TIDL_TOOLS_PATH'],
'artifacts_folder' : output_dir,
'tensor_bits' : 16,
'accuracy_level' : 0,
'advanced_options:calibration_frames' : len(calib_images),
'advanced_options:calibration_iterations' : 3 # used if accuracy_level = 1
}
so = rt.SessionOptions()
EP_list = ['TIDLCompilationProvider','CPUExecutionProvider']
sess = rt.InferenceSession(onnx_model_path ,providers=EP_list, provider_options=[compile_options, {}], sess_options=so)
I am not sure about the error. It says failure during initialization (may be memory issue.)
Can you please check.
Thanks in advance.