This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: DECODER hardware

Part Number: TDA4VM

HI, TI

  Is there a hardware or SDK restriction on 64k pages and corresponding scenarios for tda4? 64k must be used ?

The specific information is as follows:

In Processor SDK Linux J721e, DECODER hardware supports the following codecs:
• Video Decode: H.264, HEVC/H.265, MPEG4/H.263, WMV9, VC-1, MPEG2, DivX, AVS, RealVideo, VP8, VP6, Sorenson
• Image Decode: MJPEG

Support for H264 format files as described on the web page. Actually input H264 video, decoding error.

Tidec_decode supported format information is not displayed.

Tienc_encode supported formats are displayed in the help message.

Whether TI can provide relevant video footage ?

Thanks and Regards