Part Number: SK-TDA4VM
Other Parts Discussed in Thread: TDA4VM
Greetings,
As next Edge AI SDK for SK-TDA4VM is not released yet (current version is 08.00.01), please let me to point out what features would be nice to see:
1. Added support for OV5647 double camera (rPi connector), including range estimation example.
2. Added support 5GHz (20/40/80/160 MHz WB) mode for Intel 9260 Access Point and initial support of 6 GHz for Intel AX200/210.
3. Added support for booting from OSPI SPL UBOOT and load Linux from NVMe SSD.
4. Fixed I2C5 external connector (rPi) issue (change I2C config from MUX to direct link).
5. Added support of h.264 hardware encoder for GStreamer.
6. Switched LAN to WLAN packet route processing to R5F core.
This is a note, not a question.
Thanks,
Alexey