Part Number: TDA4VM
Hi TI,
I established a communication path between two J721e EVMs via MAIN_MCAN2 instance using CAN_H and CAN_L signals from J28 header on common processor board. Since the distance between the two boards is rather small (<<1m) I do not necessarily need differential signalling. So I wanted to omit the CAN transceiver (U75) and directly connect the two boards via MCAN2_TX/RX signals on J25 header according to the scheme shown in attached file in figure2.
Is this possible using MCAN module from TDA4VM?
Thanks for your help and best regards,
Felix
siemens_AP2921.pdf