This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3XEVM: Cannot Step-Debug SBL in CCS

Part Number: TDA3XEVM

NOTE: I am using CCS v.9.2 - cannot change this version of IDE.  Also using Vision SDK v.3.7 which also cannot be updated. 

I cannot get debugging to work for the TDA3X SBL.  I am using the SBL that is provided by the Vision SDK PDK library. When I connect to the C0 M4 core and load the SBL, everything looks good initially.  I see the step arrow pointing to the beginning of 'main' and I attempt to do some stepping.  This works for a few steps, then all of a sudden, I get this error:

Cortex_M4_IPU1_C0: Can't Run Target CPU: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.3.0.00003)

I changed the speed on my XDS560v2 emulator to legacy - slowest it goes to.  Nothing seems to get past this issue.  Even if I load the SBL and press the "play" button to just run the SBL, I get the same error over and over again. 

I am not sure what I need to change to make this SBL able to be reliably stepped through or breakpoint at a certain instruction in the SBL strategy.  I know that when I connect to the C0 core in CCS, I use GEL file to initialize the device, but the SBL does initialization itself similar to the GEL file... 

If I flash the SBL into QSPI - the SBL I am attempting to step-debug - it works...  I can load an AppImage and everything works as planned.  I simply cannot debug the SBL in CCS via JTAG inteface.  Anything I can provide to help diagnose this, please feel free to ask about.