Other Parts Discussed in Thread: AM3517
Hello,
I'm trying to load the default kernel from the PSP on an AM3517 on a Logic PD experimenter board. I'm running Ubuntu 9.04 on Virtual Box on Windows 7.
I think the issue is with the TFTP, as it won't get past that step. I've tried both flashing the kernel via tftp, and booting from tftp using a NFS file system as described in the getting started guides, but both instances I get the following:
AM3517_EVM # boot
BOOTP broadcast 1
DHCP client bound to address 192.168.1.83
Using DaVinci EMAC device
TFTP from server 192.168.1.80; our IP address is 192.168.1.83
Filename 'uImage'.
Load address: 0x82000000
Loading: T T T T T T T T T T T T T T T T T T T T
Retry count exceeded; starting again
Using DaVinci EMAC device
TFTP from server 192.168.1.80; our IP address is 192.168.1.83
Filename 'uImage'.
Load address: 0x82000000
Loading: T T T T T T T T T T T T T T
Abort
Wrong Image Format for bootm command
ERROR: can't get kernel image!
Here are the env variables:
AM3517_EVM # printenv
baudrate=115200
loadaddr=0x82000000
console=ttyS2,115200n8
mmcargs=setenv bootargs console=${console} root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait
nandargs=setenv bootargs console=${console} root=/dev/mtdblock4 rw rootfstype=jffs2
loadbootscript=fatload mmc 0 ${loadaddr} boot.scr
bootscript=echo Running bootscript from mmc ...; source ${loadaddr}
loaduimage=fatload mmc 0 ${loadaddr} uImage
mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr}
nandboot=echo Booting from nand ...; run nandargs; nand read ${loadaddr} 280000 400000; bootm ${loadaddr}
dieid#=155e0000000000000154417b02017017
ethact=DaVinci EMAC
ethaddr=00:50:c2:da:2f:6a
netmask=255.255.255.0
gatewayip=192.168.1.1
get_kernel=run nand_kernel
get_initrd=run nand_initrd
nand_kernel=nand read.i 0x80000000 280000 500000
nand_initrd=nand read.i 0x82000000 780000 2000000
tftp_kernel=tftpboot 0x80000000 uImage
tftp_initrd=tftpboot 0x82000000 ramdisk.gz
bootargs_rd=mem=256M console=ttyS2,115200n8 root=/dev/ram0 initrd=0x82000000,40M ramdisk_size=32768
bootargs_fs=mem=256M console=ttyS2,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2
bootargs_nfs=mem=256M console=ttyS2,115200n8 noinitrd rw root=/dev/nfs nfsroot=/mnt/nfs,nolock
addip=setenv bootargs $bootargs ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:eth0:on eth=$ethaddr
boot_rd=run get_kernel; run get_initrd; setenv bootargs $bootargs_rd; run addip; bootm 0x80000000
boot_fs=run get_kernel; setenv bootargs $bootargs_fs; run addip; bootm 0x80000000
boot_nfs=run get_kernel; setenv bootargs $bootargs_nfs; run addip; bootm 0x80000000
bootdelay=20
nfshost=192.168.1.80
rootpath=/home/engineering/workdir/filesys
stdin=serial
stdout=serial
stderr=serial
bootcmd=dhcp;bootm
serverip=192.168.1.80
bootargs=console=ttyS2,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.1.80:/home/engineering/workdir/filesys,nolock mem=256M omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y
bootfile=uImage
ipaddr=192.168.1.224
Environment size: 1987/131068 bytes
Any help or direction would be appreciated.
Thanks,
Aaron