This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need a 30MHz or lower processor with GPMC bus

I need to implement a processor design for some automotive EMI testing, and would like all clocks in the processor system to be below 30MHz.

Is there a processor with GPMC capability that can run at this low a frequency?  Including the internal clock of the processor.

The MPS series processors can run as low as 10MHz but do not support GPMC.

Thank you