This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK with DM6437

Other Parts Discussed in Thread: CCSTUDIO

Hi,

Hi,

I have got 2 DM6437 (one is transmitter and other Receiver )

Both has been connected to LAN.

With the help of one DM 6437 i captured a video and passed it via LAN , made it as preview  in the GUI (Hosp application ) , at the receiver side.

There is no option for the real time utilization of that incoming video, so that i stored it in Hard Disk at the receiver side.

 my doubt is, i need to visualize the incoming Video in the screen via DM6437 in the receiver side, in a real time cases.

OS: windows Xp

CCS: Version 3.3

image size is 120 x 160.

 

FPS : 25

for VPBE, i opened the project from the following path :

C:\dvsdk_1_01_00_15\psp_1_00_02_00\pspdrivers\system\dm6437\bios\dm6437_evm\src\video\sample\vpbe\build

similarly for the EMAC driver, as per reference guide,

Network Developer’s Kit (NDK) Support Package for EVMDM6437, i searched for EMAC driver path:

In the reference guide, its mentioned that :

· <src/hal/evmdm6437/eth_dm6437> Source code for DM6437 EMAC driver

But from the downloaded NDK, i couldn able to step forward, since path for EMAC driver has been broken :

C:\CCStudio_v3.3\ndk_1_93\packages\ti\ndk\src\hal,

after this path i couldn able to get  : evmdm6437/eth_dm6437.......

Am i moving in right way ? Is the process going right ?

pls guide me !!!!!!!!!!!!!!!!!