Part Number: TMDS64GPEVM
Other Parts Discussed in Thread: TCA6424A
Hi,
We have made the custom board based on am64x evm but we are not able to boot completely .
In our custom board we have removed TCA6424A chip and so when kernel start executing it is not able to detect the sd card although we have directly connected the sd card enable to 3.3v .
Please note that sdcard is detecting perfectly from uboot and we are able load kernel and device tree .
I just want to know what needs to be done to detect th sdcard in kernel .
U-Boot SPL 2021.01-00001-g911f54274e-dirty (Jan 25 2022 - 11:44:15 +0530)
i am in board_fit_config_name_match
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
SPL initial stack usage: 13392 bytes
Trying to boot from MMC2
Starting ATF on ARM64 core...
NOTICE: BL31: v2.5(release):08.00.00.004-dirty
NOTICE: BL31: Built : 21:46:29, Aug 10 2021
U-Boot SPL 2021.01-00001-g911f54274e-dirty (Jan 25 2022 - 11:45:40 +0530)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
Trying to boot from MMC2
U-Boot 2021.01-00001-g911f54274e-dirty (Jan 25 2022 - 11:45:40 +0530)
SoC: AM64X SR1.0
Model: Texas Instruments AM642 EVM
DRAM: dram init fired
dram init banksize fired
2 GiB
board init fired
MMC: mmc@fa10000: 0, mmc@fa00000: 1
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
beta fired
Net: Could not get PHY for ethernet@8000000: addr 0
am65_cpsw_nuss_slave ethernet@8000000: phy_connect() failed
No ethernet found.
Hit any key to stop autoboot: 2 1 0
WARNING: Could not determine device tree to use
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
49 bytes read in 1 ms (47.9 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
19137024 bytes read in 994 ms (18.4 MiB/s)
53223 bytes read in 5 ms (10.2 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 000000008fff0000, end 000000008fffffe6 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.41-g4c2eade9f7 (oe-user@oe-host) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Tue Aug 10 21:52:40 UTC 2021
[ 0.000000] Machine model: Texas Instruments AM642 EVM
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a3ffffff]
[ 0.000000] node 0: [mem 0x00000000a4000000-0x00000000a4ffffff]
[ 0.000000] node 0: [mem 0x00000000a5000000-0x00000000a57fffff]
[ 0.000000] node 0: [mem 0x00000000a5800000-0x00000000ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] cma: Reserved 512 MiB at 0x00000000c0000000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 2 pages/cpu s49880 r8192 d73000 u131072
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Built 1 zonelists, mobility grouping off. Total pages: 32736
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=fc40000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern) root=PARTUUID=355e696d-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 262144 (order: 5, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 4, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1448896K/2097152K available (10816K kernel code, 1344K rwdata, 4288K rodata, 1856K init, 758K bss, 123968K reserved, 524288K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 256 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @a4000000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x00000000a58c0000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000000a58d0000
[ 0.000000] random: get_random_bytes called from start_kernel+0x32c/0x4d4 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000005] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008525] Console: colour dummy device 80x25
[ 0.013120] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023793] pid_max: default: 32768 minimum: 301
[ 0.028593] LSM: Security Framework initializing
[ 0.033401] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[ 0.040992] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[ 0.051341] rcu: Hierarchical SRCU implementation.
[ 0.056605] Platform MSI: msi-controller@1820000 domain created
[ 0.062978] PCI/MSI: /bus@f4000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.072265] EFI services will not be available.
[ 0.077264] smp: Bringing up secondary CPUs ...
[ 0.082654] Detected VIPT I-cache on CPU1
[ 0.082691] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000
[ 0.082706] GICv3: CPU1: using allocated LPI pending table @0x00000000a58e0000
[ 0.082770] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.082903] smp: Brought up 1 node, 2 CPUs
[ 0.112296] SMP: Total of 2 processors activated.
[ 0.117109] CPU features: detected: 32-bit EL0 Support
[ 0.122382] CPU features: detected: CRC32 instructions
[ 0.135636] CPU: All CPU(s) started at EL2
[ 0.139845] alternatives: patching kernel code
[ 0.145627] devtmpfs: initialized
[ 0.157003] KASLR disabled due to lack of seed
[ 0.161848] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.171819] futex hash table entries: 512 (order: -1, 32768 bytes, linear)
[ 0.180861] pinctrl core: initialized pinctrl subsystem
[ 0.186854] DMI not present or invalid.
[ 0.191464] NET: Registered protocol family 16
[ 0.203791] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.211465] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.219490] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.228218] thermal_sys: Registered thermal governor 'step_wise'
[ 0.228223] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.234874] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.248573] ASID allocator initialised with 65536 entries
[ 0.282619] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages
[ 0.289492] HugeTLB registered 512 MiB page size, pre-allocated 0 pages
[ 0.296255] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.305112] cryptd: max_cpu_qlen set to 1000
[ 0.313369] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR1.0 JTAGID[0x0bb3802f] Detected
[ 0.322658] vsys_5v0: supplied by evm_12v0
[ 0.327307] vsys_3v3: supplied by evm_12v0
[ 0.331869] vddb_3v3_display: supplied by vsys_3v3
[ 0.337897] iommu: Default domain type: Translated
[ 0.343362] SCSI subsystem initialized
[ 0.348152] mc: Linux media interface: v0.10
[ 0.352564] videodev: Linux video capture interface: v2.00
[ 0.358310] pps_core: LinuxPPS API ver. 1 registered
[ 0.363393] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.372747] PTP clock support registered
[ 0.376789] EDAC MC: Ver: 3.0.0
[ 0.380838] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100
[ 0.387752] omap-mailbox 29040000.mailbox: omap mailbox rev 0x66fc9100
[ 0.394561] omap-mailbox 29060000.mailbox: omap mailbox rev 0x66fc9100
[ 0.402058] FPGA manager framework
[ 0.405657] Advanced Linux Sound Architecture Driver Initialized.
[ 0.413048] clocksource: Switched to clocksource arch_sys_counter
[ 0.419812] VFS: Disk quotas dquot_6.6.0
[ 0.423951] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes)
[ 0.437654] NET: Registered protocol family 2
[ 0.442374] IP idents hash table entries: 32768 (order: 2, 262144 bytes, linear)
[ 0.451409] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes, linear)
[ 0.460312] TCP established hash table entries: 16384 (order: 1, 131072 bytes, linear)
[ 0.468543] TCP bind hash table entries: 16384 (order: 2, 262144 bytes, linear)
[ 0.476269] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.483175] UDP hash table entries: 2048 (order: 0, 65536 bytes, linear)
[ 0.490116] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes, linear)
[ 0.497655] NET: Registered protocol family 1
[ 0.502745] RPC: Registered named UNIX socket transport module.
[ 0.508834] RPC: Registered udp transport module.
[ 0.513674] RPC: Registered tcp transport module.
[ 0.518483] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.525080] PCI: CLS 0 bytes, default 64
[ 0.529878] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.543268] Initialise system trusted keyrings
[ 0.548179] workingset: timestamp_bits=46 max_order=15 bucket_order=0
[ 0.559813] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.566511] NFS: Registering the id_resolver key type
[ 0.571740] Key type id_resolver registered
[ 0.576040] Key type id_legacy registered
[ 0.580219] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.587070] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.594862] 9p: Installing v9fs 9p2000 file system support
[ 0.644071] Key type asymmetric registered
[ 0.648277] Asymmetric key parser 'x509' registered
[ 0.653317] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.660877] io scheduler mq-deadline registered
[ 0.665511] io scheduler kyber registered
[ 0.672109] pinctrl-single f4000.pinctrl: 180 pins, size 720
[ 0.679097] pinctrl-single a40000.timesync-router: 512 pins, size 2048
[ 0.695478] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.719060] brd: module loaded
[ 0.730453] loop: module loaded
[ 0.734610] megasas: 07.714.04.00-rc1
[ 0.741324] libphy: Fixed MDIO Bus: probed
[ 0.747051] tun: Universal TUN/TAP device driver, 1.6
[ 0.752992] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.759415] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.765516] sky2: driver version 1.30
[ 0.770489] VFIO - User Level meta-driver version: 0.3
[ 0.776850] i2c /dev entries driver
[ 0.781659] sdhci: Secure Digital Host Controller Interface driver
[ 0.787994] sdhci: Copyright(c) Pierre Ossman
[ 0.792837] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.799883] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.806503] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.814554] optee: probing for conduit method.
[ 0.819183] optee: revision 3.12 (3d47a131)
[ 0.819823] optee: initialized driver
[ 0.830577] NET: Registered protocol family 17
[ 0.835324] 9pnet: Installing 9P2000 support
[ 0.839783] Key type dns_resolver registered
[ 0.844391] Loading compiled-in X.509 certificates
[ 0.864009] ti-sci 44043000.dmsc: ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
[ 0.906970] random: fast init done
[ 0.914964] omap_i2c 20000000.i2c: bus 0 rev0.12 at 100 kHz
[ 0.922761] pca953x 1-0022: supply vcc not found, using dummy regulator
[ 0.929720] pca953x 1-0022: using AI
[ 0.957092] pca953x 1-0022: failed writing register
[ 0.962252] pca953x: probe of 1-0022 failed with error -121
[ 0.968812] ssd1307fb 1-003c: failed to get reset gpio: -517
[ 0.974732] omap_i2c 20010000.i2c: bus 1 rev0.12 at 400 kHz
[ 0.981774] omap_i2c 20020000.i2c: bus 2 rev0.12 at 100 kHz
[ 0.988716] omap_i2c 20030000.i2c: bus 3 rev0.12 at 100 kHz
[ 0.994855] ti-sci-intr bus@f4000:bus@4000000:interrupt-controller1: Interrupt Router 5 domain created
[ 1.004541] ti-sci-intr bus@f4000:interrupt-controller0: Interrupt Router 3 domain created
[ 1.013251] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[ 1.032286] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[ 1.039992] j721e-pcie f102000.pcie: IO 0x0068001000..0x0068010fff -> 0x0068001000
[ 1.048317] j721e-pcie f102000.pcie: MEM 0x0068011000..0x006fffffff -> 0x0068011000
[ 1.056621] j721e-pcie f102000.pcie: IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[ 1.065777] ti-bcdma 485c0100.dma-controller: Number of rings: 68
[ 1.073512] ti-bcdma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6)
[ 1.083837] ti-pktdma 485c0000.dma-controller: Number of rings: 288
[ 1.097938] ti-pktdma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15)
[ 1.109213] printk: console [ttyS2] disabled
[ 1.113676] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 16, base_baud = 3000000) is a 8250
[ 1.122436] printk: console [ttyS2] enabled
[ 1.122436] printk: console [ttyS2] enabled
[ 1.130879] printk: bootconsole [ns16550a0] disabled
[ 1.130879] printk: bootconsole [ns16550a0] disabled
[ 1.143415] spi-nor spi0.0: unrecognized JEDEC id bytes: ff ff ff ff ff ff
[ 1.150343] spi-nor: probe of spi0.0 failed with error -2
[ 1.205058] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.212656] libphy: 8000f00.mdio: probed
[ 1.216816] mdio_bus 8000f00.mdio: MDIO device at address 0 is missing.
[ 1.223571] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000002
[ 1.236803] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16
[ 1.243656] am65-cpsw-nuss 8000000.ethernet: Use random MAC address
[ 1.249953] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4
[ 1.257082] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[ 1.263653] pps pps0: new PPS source ptp0
[ 1.268093] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[ 1.280662] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0
[ 1.291809] mmc0: CQHCI version 5.10
[ 1.303348] ssd1307fb 1-003c: failed to get reset gpio: -517
[ 1.309802] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[ 1.317299] j721e-pcie f102000.pcie: IO 0x0068001000..0x0068010fff -> 0x0068001000
[ 1.325402] j721e-pcie f102000.pcie: MEM 0x0068011000..0x006fffffff -> 0x0068011000
[ 1.333500] j721e-pcie f102000.pcie: IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[ 1.337103] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[ 1.350905] ssd1307fb 1-003c: failed to get reset gpio: -517
[ 1.357584] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[ 1.365179] j721e-pcie f102000.pcie: IO 0x0068001000..0x0068010fff -> 0x0068001000
[ 1.373351] j721e-pcie f102000.pcie: MEM 0x0068011000..0x006fffffff -> 0x0068011000
[ 1.381567] j721e-pcie f102000.pcie: IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[ 1.394854] debugfs: Directory 'pd:114' with parent 'pm_genpd' already present!
[ 1.409816] ALSA device list:
[ 1.412794] No soundcards found.
[ 1.416798] Waiting for root device PARTUUID=355e696d-02...
[ 1.466578] mmc0: new HS400 MMC card at address 0001
[ 1.472407] mmcblk0: mmc0:0001 W62704 3.53 GiB
[ 1.477283] mmcblk0boot0: mmc0:0001 W62704 partition 1 2.00 MiB
[ 1.483482] mmcblk0boot1: mmc0:0001 W62704 partition 2 2.00 MiB
[ 1.489660] mmcblk0rpmb: mmc0:0001 W62704 partition 3 512 KiB, chardev (237:0)
[ 1.502152] ssd1307fb 1-003c: failed to get reset gpio: -517
[ 1.508585] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[ 1.516041] j721e-pcie f102000.pcie: IO 0x0068001000..0x0068010fff -> 0x0068001000
[ 1.524168] j721e-pcie f102000.pcie: MEM 0x0068011000..0x006fffffff -> 0x0068011000
[ 1.532267] j721e-pcie f102000.pcie: IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[ 316.513201] Kernel panic - not syncing: stack-protector: Kernel stack is corrupted in: sched_move_task+0x1a0/0x1a0
[ 316.523552] CPU: 0 PID: 121 Comm: kworker/dying Not tainted 5.10.41-g4c2eade9f7 #1
[ 316.531103] Hardware name: Texas Instruments AM642 EVM (DT)
[ 316.536662] Call trace:
[ 316.539106] dump_backtrace+0x0/0x1a0
[ 316.542759] show_stack+0x18/0x68
[ 316.546068] dump_stack+0xd0/0x12c
[ 316.549459] panic+0x16c/0x334
[ 316.552507] __stack_chk_fail+0x30/0x40
[ 316.556332] cpu_cgroup_attach+0x0/0x70
[ 316.560160] sched_autogroup_exit_task+0x10/0x20
[ 316.564766] do_exit+0x300/0x9c8
[ 316.567986] kthread+0x100/0x160
[ 316.571206] ret_from_fork+0x10/0x34