This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6437 - McBSP SPI slave mode

Summary of the discussion so far:

Me:

I had a quick couple of questions about SPI in slave mode on DM6437. What is the typical setup you guys use for validating SPI in slave mode?

 

Is it –

1)      Same port in digital loop back

2)      Same port in external loop back (connecting the tx pins to corresponding rx pins)

3)      Across two different ports of DM6437

4)      With a different external SPI master

 In case it is option 4, can you also tell me what is the micro-processor that you guys usually use?

 

Sandeep of TI:

Hi Sreenath,

While validating the McBSP in SPI mode, we had a setup like in point (3). The two EVM boards are connected to each other, one is acting as a Master and other one as slave.