This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TrustZone / M-Shield



Hi

This is a follow-up on : http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/t/58680.aspx "Setup a secure world environment using Trustzone" (since the initial question already has one suggested answer it seems more rational to create a new topic for this related issue).

Is the policy regarding Trustzone the same for general purpose OMAP4x devices as for general purpose OMAP3x devices ? More precisely, is it possible to access the "secure world" (after having set up a custom security monitor or by using some built-in monitor for handling SMC calls) on a Panda Board or equivalent ? Or is the NS bit (in the Secure Configuration Register) somehow set to 1 by the first stage bootloader (ROM Code) without any possibility for the developer to set up the secure environment before this switch to the non-secure world ?

Apart from the post mentioned above, there seems to be very few hints of developers willing to use security technologies such as TrustZone and/or M-Shield on development board. Are these technologies reserved to TI's partners or are they publicly available ?

Thanks in advance,

Gabriel

  • Gabriel,

    The general purpose policy or GP device policy is same for OMAP 3x and OMAP4x devices.

    Security features are only available in OMAP HS/High Security devices and cannot be enabled in GP devices.
    Access to TI security technology including MShield/TrustZone requires a NDA license agreement with TI.

    Please contact your TI representative if you need more information about the NDA license agreement for OMAP4 HS devices.

    Regards,
    Nisha

    ---------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.

    ---------------------------------------------------------------------------------------------------------