Other Parts Discussed in Thread: OMAP-L137
hi - i'm having a similar problem [as posted here -ed] of getting stuck in a loop in the .s62 file on the EVM OMPL-137 - do you remember which were the options you had wrong? My code gets stuck at the last line of
;; ======== HWI_Obj HWI_RESET ========
;; defines function for the RESET ISR
;;
;; HWI_Obj HWI_RESET (function, monitor, addr, dataType, operation, client, iUseDispatcher, iArg, IntrMask, iCCBitMask, iLoadTrack)
.global HWI_RESET
.asg _c_int00, _function
.asg "Nothing", _monitor
.asg 00H, _addr
.asg "signed", _dataType
.asg "STS_add(*addr)", _operation
.asg "USER", _client
.asg 00H, _iUseDispatcher
.asg 00H, _iArg
.asg 01H, _IntrMask
.asg 01H, _iCCBitMask
.asg 00H, _iLoadTrack
HWI_Obj 1, HWI_RESET, 0, _function, _monitor, _addr, _dataType, _operation, _client, _iUseDispatcher, _iArg, _IntrMask, _iCCBitMask, _iLoadTrack
It used to happen randomly every once in a while in CCS3.3, but now that I've migrated to CCS4 i've only gotten past it once.
thanks,
Arvid