Part Number: TDA3MV
Hello,
which external clock input, and which internal PLLs are involved to create the timing of the external CAN-FD signals (FCLK, MCAN_CLK)?
I'm interested in calculating the overall jitter for the CAN-FD protocol. The jitter is a combination of
- ext. clock source (oscillator) jitter,
- plus the jitter of the internal PLLs (while they are accelerating/decelerating, to chase their input clock phase).
What is the overall jitter contribution from the internal PLLs, which impact the ext. CAN-FD signal timing?
Thanks and best regards,
Andre.