Part Number: AM6442
Hello,
I have a question to the RGMII timing:
AM64XX ICSSG required RGMII input slew rate
The DS (SPRSP56B – JANUARY 2021 – REVISED AUGUST 2021) specifies a req input slow rate of:

Min 2,65V/ns = 679ps @1,8V
Max 5V/ns= 360ps @1,8V
This is more tight as the RGMII spec (750ps), pls double check this!
Regards
Tom