This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Syslink Problem: ProcMgr_load hangs



Whenever I attempt to load any DSP code with IPC functions ProcMgr_load hangs.  It returns whenever I attempt to load non-IPC code.  I see:

ProcMgr Attach status = 0x97d2000

ProcMgr state after attach = 1

I'm using procId=0 for the DSP of the c6a816x EVM.  The ARM side code is copied from the ProcmgrApp example that came with EZSDK.  Syslink is version 02_00_00_56.

Am I missing something or do I simply need to wait for the beta release?

Update:

I rebuilt my ARM-side code with ProcMgr.c as part of my project and put a couple of Osal_printfs in to see what is happening.  The process is getting stuck after the call to ProcMgrDrvUsr_ioctl in the syslink.ko module.  The ioctl never returns.  I'm using the pre-built syslink.ko as it came with EZSDK.

Lee Holeva

 

  • Not sure why this is, but the app is no longer hanging, but now I'm getting an error code after load:

    root@c6a816x-evm:~/c6a816x-evm/r1397# ./runDSP_debug.xv5T DSPtasks.out
    ProcMgr_attach status: 0x97d2000
    After attach: ProcMgr_getState
        state [0x1]
    Error in ProcMgr_load: status = 0x8485f003
    Registered remote event number 10 with Notify module for processor 0
    Registered remote event number 11 with Notify module for processor 0
    Registered remote event number 12 with Notify module for processor 0
    Registered remote event number 13 with Notify module for processor 0
    Error in Notify_sendEvent for processor 0Status = -7
    Press Return to cleanup and exit

    Error in Notify_sendEvent for processor 0Status = -7
    Unregistered remote event number 10 with Notify module. Status [0x0]
    Unregistered remote event number 11 with Notify module. Status [0x0]
    Unregistered remote event number 12 with Notify module. Status [0x0]
    Unregistered remote event number 13 with Notify module. Status [0x0]
    Ipc_control Ipc_CONTROLCMD_STOPCALLBACK status = -1
    ProcMgr_stop status: [0x6a85000]
    After stop: ProcMgr_getState
        state [0x2]
    ProcMgr_unload status: [0x8485f003]
    After unload: ProcMgr_getState
        state [0x2]
    ProcMgr_detach status: [0x6a85000]
    After detach: ProcMgr_getState
        state [0x0]
    ProcMgr_close status: [0x0]

    The promgrapp that came with the EZSDK also gives an error code:

    oot@c6a816x-evm:~/c6a816x-evm/r1397# ./procmgrapp.exe 0 DSPtasks.out
    ProcMgrApp sample application
    Entered ProcMgrApp_startup
    ProcMgr_attach status: [0x97d2000]
    After attach: ProcMgr_getState
        state [0x1]
    ProcMgr_load status: [0x3046000]
    After load: Error in Ipc_control Ipc_CONTROLCMD_LOADCALLBACK: -1
    Leaving ProcMgrApp_startup
    Press enter to continue and perform shutdown ...

    Entered ProcMgrApp_shutdown
    Ipc_control Ipc_CONTROLCMD_STOPCALLBACK status: [0xffffffff]
    ProcMgr_stop status: [0x6a85000]
    After stop: ProcMgr_getState
        state [0x2]
    ProcMgr_unload status: [0x0]
    After unload: ProcMgr_getState
        state [0x2]
    ProcMgr_detach status: [0x6a85000]
    After detach: ProcMgr_getState
        state [0x0]
    ProcMgr_close status: [0x0]
    Leaving ProcMgrApp_shutdown

    I've also tried the NotifyApp example and this works only locally, the message passing fails going between the ARM and DSP.

    Lee Holeva

  • Lee

    I am getting this same error:

    root@c6a816x-evm:~/c6a816x-evm/r1397# ./runDSP_debug.xv5T DSPtasks.out
    ProcMgr_attach status: 0x97d2000
    After attach: ProcMgr_getState
        state [0x1]
    Error in ProcMgr_load: status = 0x8485f003

     

    Did you find a solution to the problem with procMgr_load()?

    Thanks.

  • Ben Clarke said:

    Did you find a solution to the problem with procMgr_load()?

     

    Origially I could not get the DSP-side code to build in EZSDK so went to CCS, but at the time I did not know about the missing Syslink rtos library, without which the code builds, but will not run.  When I figured-out how to build the DSP-side code using xdc in the SDK, with the Syslink rtos library, the problem of procMgr hanging went away.

    Lee Holeva