I have scoured all the datasheets I can find; and can not for the life of me find the base address of the EMDA3 registers! Am I missing something obvious?
The register offsets are all listed in https://www.ti.com/lit/ug/sprugp9b/sprugp9b.pdf section 4.2 (page 83) - but what is the base addresses (for both channel controller 0 and 1)?
I do see in Figure 8 (page 30) of the above document - it actually lists the Byte Address of the PaRAM sets for (I assume) EDMA Channel Controller 0 as 0x01C04000h - and I believe this to be correct as it works. But where is the address for EDMA Channel Controller 1?
There must be a place that lists the base addresses that Im missing; but Ive spent the better part of a day scouring the internet for these addresses. Can someone point me in the right direction?
Thanks