This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6747: Transition time

Guru 10095 points
Part Number: TMS320C6747

Hi Support Team,

My customer is using DA810 and he need to know the following question.
I think that DA810 is nearly equaled C6747, so I post here as C6747.

It is mentioned in the datasheet that Transition time spec. is as follow.

Recommended Operating Conditions below mention 10%-90%.

However, different part in the datasheet below mention VIL MAX & VIH MIN.

 

Does it mean for clock signal like SPI1_CLK (input signal), the spec is 0.25P or 10ns
& Transition timing is referenced from VIH MIN and VIL MAX instead of 10%-90% ?

Best regards,
Kanae