This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4VM

Part Number: TDA4VM

Hello,

I have to test peripherals like I2C, SPI, eMMC, ethernet in R5F MCU domain. I have built the u-boot(tiboot3.bin) as mentioned in  

3.1.1.1. General Information — Processor SDK Linux for J721e Documentation.

Based on whether it is for MCU or Main domain there are 2 options: 

1. If this u-boot is for R5F MCU domain, then I can test the peripheral in u-boot command prompt (For ex. using i2c probe command) 

2. If this u-boot is for R5F Main domain, is there any alternative method where I can test these peripherals in R5F  MCU domain?

Thanks in advance,

Lakshmi Shetty