This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM J721e runtime kernel panic

Hi there,

The runtime kernel panic issues have happened, and the details log as follow:

1. Master chip kernel panic log:

nice-all-RT-tasks(n) poweroff(o) show-registers(p) show-all-timers(q) unraw(r) sync(s) show-task-states(t) unmount(u) show-blocked-tasks(w)
<1>[165713.192060] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000010
<1>[165713.192063] Mem abort info:
<1>[165713.192065] ESR = 0x96000007
<1>[165713.192067] EC = 0x25: DABT (current EL), IL = 32 bits
<1>[165713.192069] SET = 0, FnV = 0
<1>[165713.192070] EA = 0, S1PTW = 0
<1>[165713.192071] Data abort info:
<1>[165713.192073] ISV = 0, ISS = 0x00000007
<1>[165713.192074] CM = 0, WnR = 0
<1>[165713.192077] user pgtable: 64k pages, 48-bit VAs, pgdp=00000008ceeb2a00
<1>[165713.192078] [0000000000000010] pgd=00000008d4d90003, pud=00000008d4d90003, pmd=00000008d3980003, pte=0000000000000000
<0>[165713.192084] Internal error: Oops: 96000007 [#1] PREEMPT SMP
<4>[165713.192087] Modules linked in: xhci_plat_hcd xhci_hcd usbcore omap_rng cdns3 rng_core roles pru_rproc udc_core usb_common irq_pruss_intc icss_iep crct10dif_ce ti_j721e_cpsw_virt_mac tipwm_driver pruss sa2ul sha512_generic authenc cdns3_ti sch_fq_codel ip_tables x_tables ipv6 pvrsrvkm(O) rpmsg_kdrv_switch rpmsg_pru virtio_rpmsg_bus rpmsg_char ti_k3_dsp_remoteproc ti_k3_r5_remoteproc
<4>[165713.192113] CPU: 0 PID: 380 Comm: iperf3 Tainted: G O 5.4.74-ACU-3.0.1.2 #4
<4>[165713.192114] Hardware name: Texas Instruments K3 J721E SoC (DT)
<4>[165713.192117] pstate: 20000005 (nzCv daif -PAN -UAO)
<4>[165713.192126] pc : virt_cpsw_nuss_tx_poll+0xb4/0x280 [ti_j721e_cpsw_virt_mac]
<4>[165713.192130] lr : virt_cpsw_nuss_tx_poll+0xa4/0x280 [ti_j721e_cpsw_virt_mac]
<4>[165713.192131] sp : ffff80001632f690
<4>[165713.192132] x29: ffff80001632f690 x28: ffff00084b9f0000
<4>[165713.192135] x27: ffff00084ea420b0 x26: ffff00084076cc10
<4>[165713.192137] x25: ffff00084ea420a8 x24: 00000000000005ea
<4>[165713.192139] x23: 000000000000003e x22: ffff00084c1a6200
<4>[165713.192141] x21: 0000000000000002 x20: 0000000000000040
<4>[165713.192143] x19: ffff00084ea420d0 x18: 0000000000000000
<4>[165713.192145] x17: 0000000000000000 x16: 0000000000000000
<4>[165713.192147] x15: 0000000000000000 x14: 6c42f5c088b441bd
<4>[165713.192150] x13: ffff800012860000 x12: 0000000000000001
<4>[165713.192152] x11: 1e865ed87b7579ac x10: 0000000000000000
<4>[165713.192155] x9 : 0000000000000003 x8 : ffff800012860038
<4>[165713.192157] x7 : 0000000000000001 x6 : 0000000000000000
<4>[165713.192160] x5 : fffffffffffffff7 x4 : ffff80086eb00000
<4>[165713.192162] x3 : 0000000000000000 x2 : 000000000000ff00
<4>[165713.192164] x1 : 000000000000003e x0 : 0000000000000000
<4>[165713.192167] Call trace:
<4>[165713.192173] virt_cpsw_nuss_tx_poll+0xb4/0x280 [ti_j721e_cpsw_virt_mac]
<4>[165713.192193] net_rx_action+0x114/0x340
<4>[165713.192202] __do_softirq+0x120/0x25c
<4>[165713.192206] do_softirq.part.0+0x60/0x68
<4>[165713.192209] __local_bh_enable_ip+0x8c/0x98
<4>[165713.192218] ip_finish_output2+0x17c/0x580
<4>[165713.192220] __ip_finish_output+0xc8/0x200
<4>[165713.192223] ip_output+0xf4/0x1a8
<4>[165713.192225] ip_local_out+0x44/0x58
<4>[165713.192228] __ip_queue_xmit+0x124/0x390
<4>[165713.192255] ip_queue_xmit+0x10/0x18 [ipv6]
<4>[165713.192259] __tcp_transmit_skb+0x448/0xa88
<4>[165713.192261] __tcp_send_ack.part.0+0xc8/0x118
<4>[165713.192263] tcp_send_ack+0x20/0x30
<4>[165713.192265] tcp_cleanup_rbuf+0x64/0x100
<4>[165713.192267] tcp_recvmsg+0x1cc/0x950
<4>[165713.192282] inet6_recvmsg+0x4c/0x118 [ipv6]
<4>[165713.192286] sock_read_iter+0x90/0xe8
<4>[165713.192292] new_sync_read+0xe4/0x178
<4>[165713.192294] __vfs_read+0x2c/0x40
<4>[165713.192298] vfs_read+0xc8/0x1a0
<4>[165713.192301] ksys_read+0x68/0xf0
<4>[165713.192303] __arm64_sys_read+0x18/0x20
<4>[165713.192308] el0_svc_common.constprop.0+0x68/0x160
<4>[165713.192311] el0_svc_handler+0x20/0x80
<4>[165713.192313] el0_svc+0x8/0x204
<0>[165713.192320] Code: f94037e3 d538d084 2a1703e1 aa0303e0 (f940087c)
<4>[165713.192325] ---[ end trace fb0da6d660b201f8 ]---
<0>[165713.193109] Kernel panic - not syncing: Fatal exception in interrupt
<2>[165713.193112] SMP: stopping secondary CPUs
<0>[165713.193123] Kernel Offset: disabled

<0>[165713.193128] CPU features: 0x0002,20006008

<0>[165713.193129] Memory Limit: none

2. Slave chip kernel panic log:

<4>[24663.834031] ------------[ cut here ]------------
<2>[24663.834039] kernel BUG at lib/genalloc.c:506!
<0>[24663.834042] Internal error: Oops - BUG: 0 [#1] PREEMPT SMP
<4>[24663.834046] Modules linked in: xhci_plat_hcd xhci_hcd usbcore omap_rng rng_core cdns3 roles udc_core usb_common pru_rproc irq_pruss_intc icss_iep ti_j721e_cpsw_virt_mac crct10dif_ce tipwm_driver pruss sa2ul cdns3_ti sha512_generic authenc sch_fq_codel ip_tables x_tables ipv6 pvrsrvkm(O) rpmsg_kdrv_switch rpmsg_pru virtio_rpmsg_bus rpmsg_char ti_k3_dsp_remoteproc ti_k3_r5_remoteproc
<4>[24663.834075] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G O 5.4.74-ACU-3.0.1.2 #4
<4>[24663.834077] Hardware name: Texas Instruments K3 J721E SoC (DT)
<4>[24663.834079] pstate: 00000005 (nzcv daif -PAN -UAO)
<4>[24663.834091] pc : gen_pool_free_owner+0xf0/0x100
<4>[24663.834093] lr : gen_pool_free_owner+0xa4/0x100
<4>[24663.834095] sp : ffff80001000fd40
<4>[24663.834096] x29: ffff80001000fd40 x28: 0000000000000040
<4>[24663.834099] x27: ffff000846dbc0b0 x26: ffff00084076cc10
<4>[24663.834101] x25: ffff000846dbc0a8 x24: 0000000000000007
<4>[24663.834104] x23: ffff00007d8800ff x22: 0000000000000000
<4>[24663.834106] x21: 0000000000000001 x20: ffff00084b1d1c00
<4>[24663.834108] x19: ffff00007d880080 x18: 0000000000000000
<4>[24663.834110] x17: 0000000000000000 x16: 0000000000000000
<4>[24663.834112] x15: 0000000000000000 x14: 0000000000000000
<4>[24663.834114] x13: ffff800011f40000 x12: 0000000000000001
<4>[24663.834116] x11: 0000000000000000 x10: 0000000000000001
<4>[24663.834119] x9 : 0000000000000001 x8 : ffff800011f40038
<4>[24663.834122] x7 : 0000000000000001 x6 : 0000000000000000
<4>[24663.834124] x5 : fffffffffffffffd x4 : 0000000000000002
<4>[24663.834126] x3 : ffff800011f40038 x2 : 0000000000000003
<4>[24663.834128] x1 : 00000000fffff000 x0 : 0000000000000001
<4>[24663.834133] Call trace:
<4>[24663.834137] gen_pool_free_owner+0xf0/0x100
<4>[24663.834168] k3_cppi_desc_pool_free

<4>[24663.834171] virt_cpsw_nuss_xmit_free.isra.0+0x60/0xf8 [ti_j721e_cpsw_virt_mac]
<4>[24663.834175] virt_cpsw_nuss_tx_poll+0xa4/0x280 [ti_j721e_cpsw_virt_mac]
<4>[24663.834188] net_rx_action+0x114/0x340
<4>[24663.834200] __do_softirq+0x120/0x25c
<4>[24663.834207] irq_exit+0xb8/0xd8
<4>[24663.834216] __handle_domain_irq+0x64/0xb8
<4>[24663.834219] gic_handle_irq+0x5c/0x148
<4>[24663.834220] el1_irq+0xb8/0x180
<4>[24663.834223] arch_cpu_idle+0x10/0x18
<4>[24663.834235] do_idle+0xc0/0x140
<4>[24663.834237] cpu_startup_entry+0x24/0x68
<4>[24663.834247] rest_init+0xd0/0xdc
<4>[24663.834252] arch_call_rest_init+0xc/0x14
<4>[24663.834254] start_kernel+0x408/0x43c
<0>[24663.834258] Code: d65f03c0 14000044 17fffff6 d4210000 (d4210000)
<4>[24663.834262] ---[ end trace 71655ce054378e36 ]---
<0>[24663.834974] Kernel panic - not syncing: Fatal exception in interrupt
<2>[24663.834977] SMP: stopping secondary CPUs
<0>[24663.834986] Kernel Offset: disabled
<0>[24663.834989] CPU features: 0x0002,20006008
<0>[24663.834990] Memory Limit: none