This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is vs DEMO in SDK a RTA program?



I'm trying to evaluate the core payload for a runtime system. And I know that oprofile/top can be utilized to measure the Cortex-A8, while another task function named "profileTskEntry" can be utilized to test thread level payload. However, the "profileTskEntry" is new in SDK, and I am thinking a way to evaluate it through CCS.

CCS has the tools named "RTA", seems satisfy my requirement. But it can be used only if the loaded program is a "RTA program". When I run the vs DEMO, I can see a prompt ("You connect the CCS now: Press any key to continue.."), seems that we can use CCS even if program is run in Linux.

Could you help confirm? both info of  v05_00_00_09 and v05_00_00_11 are  need.

Thank you

Jeff

  • Jeff,

    Here is some feedback I have received...

    Yes, VS demo can be connected to CCS after the prompt “You connect the CCS now: Press any key to continue” in both versions v05_00_00_09 and v05_00_00_11.

    I am still trying to find more out about profileTskEntry.

     

    BR,

    Steve

  • hi Steve,

    Thank you so much for your point out.

    I've tried with my blackhawk Emulator. CCS is proven OK to link with the vs demo, and I can see something in disassembling sub-windows after the Cortex-M3 for VICP is connnected. However, The RTA tools are still grey, which means it is not activated.

    I also read the source code and find the file "omx_05_00_00_11/packages/ti/omx/demos/vs2/ThrLoadCfg.cfg", in which there is some codes related with RTA. I try activate it and run the demo again to see if CCS could use RTA or not, the result is NO.

    As a result, I give up my trial of utilizing CCS RTA tools so far. If you have any good idea, pls let me know.

     

    Jeff