This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: boot pins setting for SPI FLASH BOOT MODE

Part Number: TMS320C6748
Other Parts Discussed in Thread: OMAP-L138

What is the boot pins setting for SPI FLASH BOOT MODE and how to set it

As with the SPI Writer, i got the following error:

[C674X_0] Starting OMAP-L138 SPIWriter.
Will you be writing a UBL image? (Y or y)
n
Enter the application file name (enter 'none' to skip):
C:\SecureOut.bin
    INFO: File read complete.
    ERROR: Erasing SPI failed.
SPI Flashing Failed!    SPI flashing failed!

  • Part Number: TMS320C6748

    We have used processor P/N : TMS320C6748BZWT in our board and write to SPI Flash is working.

    In the same board when we replaced the processor with P/N : TMS320C6748EZWT and tried write to the SPI Flash by connecting emulator with the SPI Writer, we are getting the following error:

    [C674X_0] Starting OMAP-L138 SPIWriter.
    Will you be writing a UBL image? (Y or y)
    n
    Enter the application file name (enter 'none' to skip):
    C:\SecureOut.bin
        INFO: File read complete.
        ERROR: Erasing SPI failed.
    SPI Flashing Failed!    SPI flashing failed!

    how can i fix this?

    The SPI flash Configuration is same and we have observed no activity on SPI lines  (cs, clk, simo, somi)

  • Hello,

    Please check the instructions for spi flashing here

    Please also note that TI does not support bare-metal or TI-RTOS based SW development for C6748/OMAP-L138 anymore, as announced here. I would recommend you to check the consolidated resources provided in the announcement.

    Regards,

    Jianzhong