Other Parts Discussed in Thread: OMAP-L138, AM1808
Hi
looking at the datasheet for this device http://focus.ti.com/lit/ds/sprs226m/sprs226m.pdf
page 131 seems to indicate that the timer speed is the system clock reduced by a factor of 8, is that correct?
I am trying to find a device that will give me a wide range of frequencies for us in PWM from 0.1MHz to 50MHz with a high resolution duty cycle over those frequencies which will require timers running close to 1GHz. If my above assumption is correct is there a device anyone can recommend that will give me these timer timings or PWM capabilities?This is the main requirement of any device for this, other requirements are secondary to this only.
Thanks