This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Failed to boot A72

Part Number: TDA4VM

Dear expert,

    When I ported the "ti-processor-sdk-rtos-j721e-evm-07_03_00_07\mcusw\mcuss_demos\boot_app_mcu_rtos" to my autosar project, I found that the A72 has booted but stopped in the SPL. We have no idea how to solve it for weeks, could you help me? Here is the log of the main domain.

 

NOTICE:  BL31: Built : 00:15:40, Apr 10 2021

ERROR:   GTC_CNTFID0 is 0! Assuming 200000000 Hz. Fix Bootloader

 

U-Boot SPL 2020.01 (Dec 29 2021 - 17:08:10 +0800)

SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')

Reading on-board EEPROM at 0x50 failed 1

Trying to boot from MMC1

ti_sci_clk_set_parent: get_num_parents failed (-19)

spl: could not initialize mmc. error: -19

SPL: failed to boot from all boot devices

### ERROR ### Please RESET the board ###