This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6548: AM6548

Part Number: AM6548

I am trying to do a yocto build for the AM65xx board so that I can a new library Libbpf, but the build was not successful, I have the following errors:

Summary: 4 tasks failed:

  /home/ubuntu/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/sources/meta-psdkla/recipes-core/packagegroups/onnxruntime.bb:do_fetch

  /home/ubuntu/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/sources/meta-arago/meta-arago-extras/recipes-devtools/input-utils/input-utils_1.0.bb:do_compile

  /home/ubuntu/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/sources/meta-qt5/recipes-qt/qt5/qtwebkit_git.bb:do_compile

  /home/ubuntu/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/sources/meta-openembedded/meta-oe/recipes-devtools/nodejs/nodejs_12.21.0.bb:do_compile

Summary: There were 7 WARNING messages shown.

Summary: There were 7 ERROR messages shown, returning a non-zero exit code.

 

Is there a way to work around this. Or is there any plans in the future to support libbpf for the AM65xx boards Linux SDKs. This may be helpful for both our companies, because our customers are waiting for the integrated library so that it can be a part of the EtherCAT master.

Best Regards

HAithem Jebali

Acontis Technologies