Part Number: TDA4VM
Dear experts,
Recently we encountered a TDA4 sdhci issue on our own PCB board, when booting from uboot to linux kernel, eMMC card can't be configured to hs200 or other wanted timing mode successfully at -40 Celsius, but when the board is warming up to -20 Celsius, eMMC catd can be successfully configured.
We have done these test as below to narrow down the scope of the problem:
1. Soldering an eMMC card which have been tested normal at-40 Celsius to the abnormal board, the abnormal board is still not able to configure eMMC successfully at -40 Celsius.
2. Soldering the TDA4 of the abnormal board to a normal board, the board will not be able to configure eMMC successfully at -40 Celsius.
The tests above shows that the problem is caused by the TDA4, the detailed log is in the attachment, does TI have the -40 Celsius test report of TDA4 sdhci? Can you help us to analyze the reason of this phenomenon?
20220214_-40_abnormal.log
Best Regards
Nathan