Part Number: PROCESSOR-SDK-AMIC110
We would like to avoid using the external DDR to reduce potential problems with EMC.
So we modified our lds to this:
/****************************************************************************/
/* AM335x.lds */
/* Copyright (c) 2014 Texas Instruments Incorporated */
/* Author: Rafael de Souza */
/* */
/* Description: This file is a sample linker command file that can be */
/* used for linking programs built with the GCC compiler */
/* and running the resulting .out file on an AM335x device. */
/* Use it as a guideline. You will want to */
/* change the memory layout to match your specific */
/* target system. You may want to change the allocation */
/* scheme according to the size of your program. */
/* */
/****************************************************************************/
MEMORY
{
SRAM : o = 0x402F0400, l = 0x0000FC00 /* 64kB internal SRAM */
L3OCMC0 : o = 0x40300000, l = 0x00010000 /* 64kB L3 OCMC SRAM */
M3SHUMEM : o = 0x44D00000, l = 0x00004000 /* 16kB M3 Shared Unified Code Space */
M3SHDMEM : o = 0x44D80000, l = 0x00002000 /* 8kB M3 Shared Data Memory */
DDR0 : o = 0x80000000, l = 0x40000000 /* 1GB external DDR Bank 0 */
}
/* Linker script to place sections and symbol values. Should be used together
* with other linker script that defines memory region DDR0.
* It references following symbols, which must be defined in code:
* Entry : Entry of reset handler
*
* It defines following symbols, which code can use without definition:
* __exidx_start
* __exidx_end
* __etext
* __data_start__
* __preinit_array_start
* __preinit_array_end
* __init_array_start
* __init_array_end
* __fini_array_start
* __fini_array_end
* __data_end__
* __bss_start__
* __bss_end__
* __end__
* end
* __HeapLimit
* __HeapBase - To be compatible with Linaro's semihosting support
* __StackLimit
* __StackTop
* __StackBase - To be compatible with Linaro's semihosting support
* __stack
*/
ENTRY(Entry)
SECTIONS
{
.rsthand :
{
. = ALIGN(0x10000);
KEEP(*(.isr_vector))
*startup_ARMCA8.o (.text)
} > L3OCMC0
. = ALIGN(4);
.text :
{
*(.text*)
KEEP(*(.init))
KEEP(*(.fini))
/* .ctors */
*crtbegin.o(.ctors)
*crtbegin?.o(.ctors)
*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors)
*(SORT(.ctors.*))
*(.ctors)
/* .dtors */
*crtbegin.o(.dtors)
*crtbegin?.o(.dtors)
*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors)
*(SORT(.dtors.*))
*(.dtors)
*(.rodata*)
KEEP(*(.eh_frame*))
} > L3OCMC0
.ARM.extab :
{
*(.ARM.extab* .gnu.linkonce.armextab.*)
} > L3OCMC0
__exidx_start = .;
.ARM.exidx :
{
*(.ARM.exidx* .gnu.linkonce.armexidx.*)
} > L3OCMC0
__exidx_end = .;
.data :
{
. = ALIGN(4);
__data_start__ = .;
*(vtable)
*(.data*)
. = ALIGN(4);
/* preinit data */
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP(*(.preinit_array))
PROVIDE_HIDDEN (__preinit_array_end = .);
. = ALIGN(4);
/* init data */
PROVIDE_HIDDEN (__init_array_start = .);
KEEP(*(SORT(.init_array.*)))
KEEP(*(.init_array))
PROVIDE_HIDDEN (__init_array_end = .);
. = ALIGN(4);
/* finit data */
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP(*(SORT(.fini_array.*)))
KEEP(*(.fini_array))
PROVIDE_HIDDEN (__fini_array_end = .);
. = ALIGN(4);
/* All data end */
__data_end__ = .;
} > M3SHUMEM
.bss :
{
. = ALIGN(4);
__bss_start__ = .;
*(.bss*)
*(COMMON)
__bss_end__ = .;
} > M3SHUMEM
.heap (NOLOAD):
{
/* The line below can be used to FILL the memory with a known value and
* debug any stack overruns. For this to work, the specifier (NOLOAD) above
* must be removed at the expense of an increase in the output binary size */
FILL(0xDEADBEEF)
. = ALIGN(4);
__end__ = .;
end = __end__;
/* The line below created to be compatible with Linaro's semihosting support */
__HeapBase = __end__;
*(.heap*)
. = . + HEAPSIZE;
__HeapLimit = .;
} > SRAM
/* .stack section doesn't contain any symbols. It is only
* used for linker to calculate size of stack sections, and assign
* values to stack symbols later */
.stack (NOLOAD):
{
/* The line below can be used to FILL the memory with a known value and
* debug any stack overruns. For this to work, the specifier (NOLOAD) above
* must be removed at the expense of an increase in the output binary size */
FILL(0xBAD0BAD0)
. = ALIGN(4);
__StackLimit = . ;
*(.stack*)
. = . + STACKSIZE;
__StackTop = . ;
/* The line below created to be compatible with Linaro's semihosting support */
__StackBase = . ;
} > L3OCMC0
PROVIDE(__stack = __StackTop);
}
/**************************************************************************/
The problem is when we move the Stack from DDR to L3OCMC0 we can't launch it any more.
I also don't quite understand how the sbl loader will load this? Is the generated bin file from CCS Capable to split this up correctly or do i need a custom script that generates one bin file for each section?