sir,
i want to know that in this processor CMOS camera are used or some other and how many camera can i use in this at a time.
regards
Ravi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
sir,
i want to know that in this processor CMOS camera are used or some other and how many camera can i use in this at a time.
regards
Ravi
Ravi,
It is very much dependent on the interface format from your camera.
There are 2 types of port which can be used.
1) ISS, which can accept up to 16 bit raw and/or YCbCr 8/16 bit or ITU656/1120. This input can be processed through the VICP which can do things like Bayer pattern interpolation, bad pixel correction etc...
2) HDVPSS which has 2 ports and can accept up to 24 bit parallel in RGB or YUV formats in various formats (656/1120, discrete syncs etc...) These ports can be further split and multiplexed in order to capture image data from up to 16 ITU656 streams.
BR,
Steve
picking up on this discussion:
Just to make sure I understand:
Using the HDVPSS I would be able to attach any sensor as long as the dataformat is video with discrete syncs and as long as the datarates are below 160Msamples/sec?
Or is there a limitation in the video line lenght? i.e. 1920 pixels per line....
Thanks
Best regards
Alf
Alf,
Yers, there are some size limits but I can't recall at the moment what they are, and I am out of the country.
I will try to get someone else to respond whilst I am out.
On the 814x there is also the option of using the camera port but I am not 100% sure what the software support status is currently.
BR,
Steve