This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

impoting project into ccs4 yields "error NO CHIP"

Hi.

Importing the  Emifa_ReadWrite_example.pjt into CCS4  ,

Trying the build all gives the error

Description  -  #error NO CHIP DEFINED (use -dCHIP_XXXX where XXXX is chip number, i.e. 6201)

On Element - csl_chiphal.h

In Folder -  e:/CCSTUD~1.3/C6000/csl/include

 

Please Advise.

 

Ephraim Oved

  • Ephraim Oved,

    Either you are using the wrong CSL for the device or you need to have a -define for the chip in the linker's build options.

    From what or where did you import this project?

    Which version of CCSv4 are you using?

    Which DSP are you using?

    Regards,
    RandyP

     

    If you need more help, please reply back. If this answers the question, please click  Verify Answer  , below.