Hi,
I konw dm6467 vpif only support clock up to 99MHz.The following is an old post:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/p/6306/23763.aspx#23763
I want to use dm6467t vpif to capture a 1080p video through raw mode.
Dm6467t vpif can support clock up to 150MHz.
My idea is that 1080p60 clock is 74.25MHz,24bit/pix, I use the raw mode with 12bit width,use two clocks to
receive one pix.Is it possible?
zcliang