This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Noise problem after Frame Buffer enlargement



Hi everyone,

    I tried to enlarge frame buffer size in boot argument as following:

Before:

video=davincifb:osd0=720x576x16,2500K

After:

video=davincifb:osd0=1024x768x16,3072K

 

After this change, there will be some noises on screen during earlier stage, and the system will always work slowly.

1. Is there any other section should be modified to fit this change in IPNC code structure?

2. Is there any constraint about frame buffer size?

3. Is there any method to relieve the situation if OSD0 in 1024x768 is needed?

[System Information]

 

DM368

 

DVSDK_2_10_01_18

 

linux-2.6.18_pro500

 

framework_components_2_25_00_04

 

linuxutils_2_24_03