Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J721E: tda4 cpsw9g ethernet does not work

Part Number: PROCESSOR-SDK-J721E
Other Parts Discussed in Thread: 4460

Hi team,

The customer use the PROCESSOR SDK 7.3  linux+rtos. They need to use the RGMII1 and RGMII2.

When manually config the IP for eth0 on A72 side,it will show the errors as below.

Could you help to debug it?

root@j7-evm:~# ifconfig
eth0      Link encap:Ethernet  HWaddr 70:FF:76:1D:92:C1   
         inet6 addr: fe80::72ff:76ff:fe1d:92c1/64 Scope:Link
         UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
         RX packets:0 errors:0 dropped:0 overruns:0 frame:0
         TX packets:26 errors:0 dropped:0 overruns:0 carrier:0
         collisions:0 txqueuelen:1000  
         RX bytes:0 (0.0 B)  TX bytes:4460 (4.3 KiB)

lo        Link encap:Local Loopback   
         inet addr:127.0.0.1  Mask:255.0.0.0
         inet6 addr: ::1/128 Scope:Host
         UP LOOPBACK RUNNING  MTU:65536  Metric:1
         RX packets:82 errors:0 dropped:0 overruns:0 frame:0
         TX packets:82 errors:0 dropped:0 overruns:0 carrier:0
         collisions:0 txqueuelen:1000  
         RX bytes:6220 (6.0 KiB)  TX bytes:6220 (6.0 KiB)

root@j7-evm:~# [  126.359475] Initializing XFRM netlink socket
[  129.985335] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to l
oad br_netfilter if you need this.
[  129.999281] Bridge firewalling registered

root@j7-evm:~# ifconfig eth0 192.168.3.111 netmask 255.255.254.0
[ 1196.047014] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0: register_ipv4 rpmsg - fail -5
[ 1196.056088] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0: unregister_ipv4 rpmsg - fail -5
[ 1196.065457] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0: register_ipv4 rpmsg - fail -5

 logs on MCU2_0:

root@j7-evm:/opt/vision_apps# [MCU2_0]      3.959023 s: CIO: Init ... Done !!!
[MCU2_0]      3.959089 s: ### CPU Frequency <ORG = 1000000000 Hz>, <NEW = 1000000000 Hz>
[MCU2_0]      3.959130 s: APP: Init ... !!!
[MCU2_0]      3.959149 s: SCICLIENT: Init ... !!!
[MCU2_0]      3.959339 s: SCICLIENT: DMSC FW version [21.1.1--v2021.01a (Terrific Lla]
[MCU2_0]      3.959374 s: SCICLIENT: DMSC FW revision 0x15   
[MCU2_0]      3.959397 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU2_0]      3.959421 s: SCICLIENT: Init ... Done !!!
[MCU2_0]      3.959441 s: UDMA: Init ... !!!
[MCU2_0]      3.960495 s: UDMA: Init ... Done !!!
[MCU2_0]      3.960539 s: MEM: Init ... !!!
[MCU2_0]      3.960571 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ e1000000 of size 16777216
bytes !!!
[MCU2_0]      3.960625 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 3600000 of size 131072 bytes !!!
[MCU2_0]      3.960670 s: MEM: Created heap (DDR_NON_CACHE_ME, id=5, flags=0x00000000) @ d8000000 of size 1677721
6 bytes !!!
[MCU2_0]      3.960714 s: MEM: Init ... Done !!!
[MCU2_0]      3.960733 s: IPC: Init ... !!!
[MCU2_0]      3.960762 s: IPC: 6 CPUs participating in IPC !!!
[MCU2_0]      3.960796 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU2_0]     16.020322 s: IPC: HLOS is ready !!!
[MCU2_0]     16.025970 s: IPC: appIpcCreateRpmsgRxTask ok!!!
[MCU2_0]     16.026518 s: ####### IPC: appIpcCreateRpmsgTxTask ok!!!
[MCU2_0]     16.026568 s: IPC: Init ... Done !!!
[MCU2_0]     16.026590 s: APP: Syncing with 5 CPUs ... !!!
[MCU2_0]     16.026626 s: APP: Syncing with 5 CPUs ... Done !!!
[MCU2_0]     16.026653 s: REMOTE_SERVICE: Init ... !!!
[MCU2_0]     16.028288 s: REMOTE_SERVICE: Init ... Done !!!
[MCU2_0]     16.028353 s: ETHFW: Init ... !!!
[MCU2_0]     16.047733 s: CPSW_9G Test on MAIN NAVSS
[MCU2_0]     16.059814 s: PHY 1 is alive
[MCU2_0]     16.059878 s: PHY 3 is alive
[MCU2_0]     16.064416 s: ETHFW: Version   : 0.01.01 VT102 | 脱机 | ttyUSB0                                      
                                                         [MCU2_0]     16.064471 s: ETHFW: Build Date: Feb 17, 20
22
[MCU2_0]     16.064499 s: ETHFW: Build Time: 16:04:22
[MCU2_0]     16.064522 s: ETHFW: Commit SHA: e0cd30cd
[MCU2_0]     16.064547 s: ETHFW: Init ... DONE !!!
[MCU2_0]     16.064571 s: ETHFW: Remove server Init ... !!!
[MCU2_0]     16.065798 s: Remote demo device (core : mcu2_0) .....
[MCU2_0]     16.065855 s: ETHFW: Remove server Init ... DONE !!!
[MCU2_0]     16.071509 s: Host MAC address: 70:ff:76:1d:92:c2
[MCU2_0]     16.115070 s: FVID2: Init ... !!!
[MCU2_0]     16.115180 s: FVID2: Init ... Done !!!
[MCU2_0]     16.115251 s: ###appI2cInit: i2c 0 Address 0x40b00000
[MCU2_0]     16.115303 s: ###appI2cInit: i2c 1 Address 0x40b10000
[MCU2_0]     16.115347 s: ###appI2cInit: i2c 2 Address 0x0
[MCU2_0]     16.115387 s: ###appI2cInit: i2c 3 Address 0x0
[MCU2_0]     16.115426 s: ###appI2cInit: i2c 4 Address 0x0
[MCU2_0]     16.115465 s: ###appI2cInit: i2c 5 Address 0x0
[MCU2_0]     16.115503 s: ###appI2cInit: i2c 6 Address 0x0
[MCU2_0]     16.115533 s: ##### APP: appI2cInit !!!
[MCU2_0]     16.115555 s: ############ APP: Init  ENABLE_DSS_EDP ... !!!
[MCU2_0]     16.115580 s: ~~~~~~~~ DISPLAY resolution 1440X900 ~~~~~~~~~~
[MCU2_0]     16.115605 s: DSS: Init ... !!!
[MCU2_0]     16.115621 s: DSS: Display type is eDP !!!
[MCU2_0]     16.115640 s: DSS: SoC init ... !!!
[MCU2_0]     16.115657 s: SCICLIENT: Sciclient_pmSetModuleState module=152 state=2
[MCU2_0]     16.115821 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.115854 s: SCICLIENT: Sciclient_pmSetModuleState module=297 state=2
[MCU2_0]     16.115988 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.116013 s: SCICLIENT: Sciclient_pmSetModuleState module=151 state=2
[MCU2_0]     16.116112 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.116142 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=9 parent=11
[MCU2_0]     16.116224 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_0]     16.116251 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=13 parent=18
[MCU2_0]     16.116316 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_0]     16.116342 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=1 parent=2
[MCU2_0]     16.116405 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_0]     16.116430 s: SCICLIENT: Sciclient_pmSetModuleClkFreq module=152 clk=1 freq=106500000
[MCU2_0]     16.117407 s: SCICLIENT: Sciclient_pmSetModuleClkFreq success
[MCU2_0]     16.117438 s: SCICLIENT: Sciclient_pmModuleClkRequest module=152 clk=1 state=2 flag=0
[MCU2_0]     16.117543 s: SCICLIENT: Sciclient_pmModuleClkRequest success
[MCU2_0]     16.117570 s: DSS: SoC init ... Done !!!
[MCU2_0]     16.117589 s: DSS: Board init ... !!!
[MCU2_0]     16.117606 s: DSS: Board init ... Done !!!
[MCU2_0]     16.122257 s: Function:CpswProxyServer_attachExtHandlerCb,HostId:0,CpswType:6
[MCU2_0]     16.135733 s: DSS: Init ... Done !!!
[MCU2_0]     16.135793 s: appInit APP: Init line 690 ... !!!
[MCU2_0]     16.135835 s: appInit APP: Init line 719 ... !!!
[MCU2_0]     16.135863 s: VHWA: VPAC Init ... !!!
[MCU2_0]     16.135881 s: SCICLIENT: Sciclient_pmSetModuleState module=290 state=2
[MCU2_0]     16.136100 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.136134 s: VHWA: LDC Init ... !!!
[MCU2_0]     16.138951 s: VHWA: LDC Init ... Done !!!
[MCU2_0]     16.138998 s: VHWA: MSC Init ... !!!
[MCU2_0]     16.147183 s: VHWA: MSC Init ... Done !!!
[MCU2_0]     16.147230 s: VHWA: NF Init ... !!!
[MCU2_0]     16.148649 s: VHWA: NF Init ... Done !!!
[MCU2_0]     16.148693 s: VHWA: VISS Init ... !!!
[MCU2_0]     16.154428 s: VHWA: VISS Init ... Done !!!
[MCU2_0]     16.154477 s: VHWA: VPAC Init ... Done !!!
[MCU2_0]     16.154513 s:  VX_ZONE_INIT:Enabled
[MCU2_0]     16.154537 s:  VX_ZONE_ERROR:Enabled
[MCU2_0]     16.154558 s:  VX_ZONE_WARNING:Enabled
[MCU2_0]     16.155613 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target IPU1-0  
[MCU2_0]     16.155881 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target VPAC_NF  
[MCU2_0]     16.156198 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target VPAC_LDC1  
[MCU2_0]     16.156471 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target VPAC_MSC1  
[MCU2_0]     16.156723 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target VPAC_MSC2  
[MCU2_0]     16.157001 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target VPAC_VISS1  
[MCU2_0]     16.157352 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target CAPTURE1  
[MCU2_0]     16.157643 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target CAPTURE2  
[MCU2_0]     16.157944 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target DISPLAY1  
[MCU2_0]     16.158311 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target DISPLAY2  
[MCU2_0]     16.158587 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target CSITX  
[MCU2_0]     16.158865 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target CAPTURE3  
[MCU2_0]     16.159207 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target CAPTURE4  
[MCU2_0]     16.159505 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target CAPTURE5  
[MCU2_0]     16.159801 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target CAPTURE6  
[MCU2_0]     16.160105 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target CAPTURE7  
[MCU2_0]     16.160396 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:55] Added target CAPTURE8  
[MCU2_0]     16.160443 s:  VX_ZONE_INIT:[tivxInit:71] Initialization Done !!!
[MCU2_0]     16.160471 s: APP: OpenVX Target kernel init ... !!!
[MCU2_0]     16.172438 s: APP: OpenVX Target kernel init ... Done !!!
[MCU2_0]     16.172488 s: CSI2RX: Init ... !!!
[MCU2_0]     16.172507 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2
[MCU2_0]     16.172591 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.172620 s: SCICLIENT: Sciclient_pmSetModuleState module=26 state=2
[MCU2_0]     16.172712 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.172737 s: SCICLIENT: Sciclient_pmSetModuleState module=27 state=2
[MCU2_0]     16.172812 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.172834 s: SCICLIENT: Sciclient_pmSetModuleState module=147 state=2
[MCU2_0]     16.172893 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.172917 s: SCICLIENT: Sciclient_pmSetModuleState module=148 state=2
[MCU2_0]     16.172975 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.173650 s: CSI2RX: Init ... Done !!!
[MCU2_0]     16.173697 s: CSI2TX: Init ... !!!
[MCU2_0]     16.173719 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2
[MCU2_0]     16.173789 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.173816 s: SCICLIENT: Sciclient_pmSetModuleState module=28 state=2
[MCU2_0]     16.173903 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.173927 s: SCICLIENT: Sciclient_pmSetModuleState module=296 state=2
[MCU2_0]     16.174002 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.174514 s: CSI2TX: Init ... Done !!!
[MCU2_0]     16.174554 s: ISS: Init ... !!!
[MCU2_0]     16.174603 s: IssSensor_Init: ret 0
[MCU2_0]     16.174633 s: IssSensor_Init ... Done !!!
[MCU2_0]     16.174708 s: vissRemoteServer_Init ... Done !!!
[MCU2_0]     16.174761 s: IttRemoteServer_Init ... Done !!!
[MCU2_0]     16.174788 s: UDMA Copy: Init ... !!!
[MCU2_0]     16.176253 s: UDMA Copy: Init ... Done !!!
[MCU2_0]     16.176304 s: APP: Init ... Done !!!
[MCU2_0]     16.176327 s: APP: Run ... !!!
[MCU2_0]     16.176346 s: APP: Run ... Done !!!
[MCU2_0]     16.176391 s: ##### mcspi_slave_init: Starting SPI Slave test.  
[MCU2_0]     16.180153 s: SPI instance 4 channel 0
[MCU2_0]     17.338732 s: Function:CpswProxyServer_registerMacHandlerCb,HostId:0,Handle:a30849fc,CoreKey:38acb7e6
, MacAddress:70:ff:76:1d:92:c1, FlowIdx:172, FlowIdxOffse0
[MCU2_0]     17.341773 s: Cpsw_ioctlInternal: CPSW: Registered MAC address.ALE entry:13, Policer Entry:0
[MCU2_0]    184.181176 s: DHCP client timed out. Retrying.....  
[MCU2_0]    352.181174 s: DHCP client timed out. Retrying.....  
[MCU2_0]    520.181193 s: DHCP client timed out. Retrying.....  
[MCU2_0]    688.181177 s: DHCP client timed out. Retrying.....  
[MCU2_0]    856.181174 s: DHCP client timed out. Retrying.....  
[MCU2_0]   1024.181177 s: DHCP client timed out. Retrying.....  
[MCU2_0]   1192.181179 s: DHCP client timed out. Retrying.....  
[MCU2_0]   1202.764369 s: Function:CpswProxyServer_registerIpv4MacHandlerCb,HostId:0,Handle:a30849fc,CoreKey:38ac
b7e6, MacAddress:70:ff:76:1d:92:c1 IPv4Addr:192.168.3.111
[MCU2_0]   1202.764546 s: Failed to add Static ARP Entry  
[MCU2_0]   1202.764587 s:  
[MCU2_0] ================LLI Table entries===========  
[MCU2_0]   1202.764613 s:  
[MCU2_0] Number of Static ARP Entries: 0  
[MCU2_0]   1202.764634 s:  
[MCU2_0] SNo.      IP Address         MAC Address   
[MCU2_0]   1202.764658 s: ------    -------------      ---------------  
[MCU2_0]   1202.773549 s: Function:CpswProxyServer_unregisterIpv4MacHandlerCb,HostId:0,Handle:a30849fc,CoreKey:38
acb7e6,IPv4Addr:c0:a8:3:6f
[MCU2_0]   1202.773655 s: Failed to add Static ARP Entry  
[MCU2_0]   1202.773693 s:  
[MCU2_0] ================LLI Table entries===========  
[MCU2_0]   1202.773720 s:  
[MCU2_0] Number of Static ARP Entries: 0  
[MCU2_0]   1202.773743 s:  
[MCU2_0] SNo.      IP Address         MAC Address   
[MCU2_0]   1202.773768 s: ------    -------------      ---------------  
[MCU2_0]   1202.782633 s: Function:CpswProxyServer_registerIpv4MacHandlerCb,HostId:0,Handle:a30849fc,CoreKey:38ac
b7e6, MacAddress:70:ff:76:1d:92:c1 IPv4Addr:192.168.3.111
[MCU2_0]   1202.782785 s: Failed to add Static ARP Entry  
[MCU2_0]   1202.782823 s:  
[MCU2_0] ================LLI Table entries===========  
[MCU2_0]   1202.782853 s:  
[MCU2_0] Number of Static ARP Entries: 0  
[MCU2_0]   1202.782876 s:  
[MCU2_0] SNo.      IP Address         MAC Address   
[MCU2_0]   1202.782899 s: ------    -------------      ---------------  
[MCU2_0]   1360.181192 s: DHCP client timed out. Retrying....

Thanks!

Best Regards,

Cherry

  • Hi,

    May I know is there any update?

    Thanks,

    Cherry

  • Hi Cherry,

    From the logs, it appears the customer wanted to use static IP.

    However, EthFW had the DHCP service enabled.

    In ndk.cfg under vision_apps/apps/basic_demos/app_tirtos/bios_cfg/ folder, please set "enableStaticIP" to 1.

    After the change, please rebuild and update the MCU2_0 firmware binary.

    [MCU2_0] ================LLI Table entries===========  
    [MCU2_0]   1202.764613 s:  
    [MCU2_0] Number of Static ARP Entries: 0  
    [MCU2_0]   1202.764634 s:  
    [MCU2_0] SNo.      IP Address         MAC Address   
    [MCU2_0]   1202.764658 s: ------    -------------      ---------------  
    [MCU2_0]   1202.773549 s: Function:CpswProxyServer_unregisterIpv4MacHandlerCb,HostId:0,Handle:a30849fc,CoreKey:38
    acb7e6,IPv4Addr:c0:a8:3:6f
    [MCU2_0]   1202.773655 s: Failed to add Static ARP Entry  
    [MCU2_0]   1202.773693 s:  
    [MCU2_0] ================LLI Table entries===========  
    [MCU2_0]   1202.773720 s:  
    [MCU2_0] Number of Static ARP Entries: 0  
    [MCU2_0]   1202.773743 s:  
    [MCU2_0] SNo.      IP Address         MAC Address   
    [MCU2_0]   1202.773768 s: ------    -------------      ---------------  
    [MCU2_0]   1202.782633 s: Function:CpswProxyServer_registerIpv4MacHandlerCb,HostId:0,Handle:a30849fc,CoreKey:38ac
    b7e6, MacAddress:70:ff:76:1d:92:c1 IPv4Addr:192.168.3.111
    [MCU2_0]   1202.782785 s: Failed to add Static ARP Entry  
    [MCU2_0]   1202.782823 s:  
    [MCU2_0] ================LLI Table entries===========  
    [MCU2_0]   1202.782853 s:  
    [MCU2_0] Number of Static ARP Entries: 0  
    [MCU2_0]   1202.782876 s:  
    [MCU2_0] SNo.      IP Address         MAC Address   
    [MCU2_0]   1202.782899 s: ------    -------------      ---------------  
    [MCU2_0]   1360.181192 s: DHCP client timed out. Retrying....

    Regards,
    Stanley

  • Hi Stanley,

    Thanks for your help.

       Currently the static IP can be used.  The customer has searched on the forum, and some threads said linux/qnx must config the ip after MCU2_0 finish the ip config.

    They would like to know the sdk how to handle the remote cores config the ip at the same time. And A72 how to know the MCU2_0 already finished the ip config?

    Thanks and regards,

    Cherry

  • Hi,

    May I know is there any update?

    Thanks and regards,

    Cherry

  • Cherry,

    EthFW will be ready when Linux command prompt is reached.

    At that point, ip address can be assigned to virt mac interface. 

    Virtual mac driver won't be up if EthFW is not ready.

    Regards,
    Stanley