This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Beagle xM Rev A -- USB, Ethernet not working



Hello,

I am trying to build root file system for Beagle xM Rev A using the following url.

http://processors.wiki.ti.com/index.php?title=Creating_a_Root_File_System_for_Linux_on_OMAP35x

I am using following url to build u-boot, MLO, uImage for the above board

http://elinux.org/BeagleBoard#Source

The board boots up with command prompt, but the board failed to identify USB pendrive and Ethernet. Pls find the attached bootup log 6305.log.txt

I tried with both mdev and udev-141 version, in both cases the /dev directory is populated, but inserting pen drive, or ethernet does not have any effect

Whereas, the default root file system and the uImage, MLO etc that comes with the board easily recognize the pendirve and ethernet.

Any help will be highly appreciated.

Regards,

Batsayan Das