This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suggestion of a MCU for 2-channel camera input and display at same time

Other Parts Discussed in Thread: TDA4VM

Hi Champ

Any suggerstion for MCU/MPU which support 2-channel camera input and display at same time?

Customer uses TDA4VM for SVM. they also need light CPU which able to support 2-channel camera input and display at same time to be used as like dashcam.

Camera type(MIPI, Parallel) and resolutions are not determnined. 

Non-Linux product is preferred. 

Regards, 

Jack 

  • Hi Jack,

    AM273x integrates two, 4-lane MIPI CSI-2, D-PHY receiver peripherals: CSI2 receiver 0 (CSI2_RX0) and CSI2 receiver 1 (CSI2_RX1). Each peripheral can be used for capturing sensor data samples. The CSI2 interface is also capable of operating as a hardware-in-the-loop (HIL) interface, allowing for the playback of recorded data for development or diagnostic purposes. • Interface is compliant with the MIPI CSI-2 D-PHY standard revision 1.2 • 2, 4-lane CSI2 receiver interfaces, working simultaneously at 600 Mbps/lane • 4-lane, 3-lane, 2-lane, or 1-lane CSI2 configurations • Support for virtual channels (minimum 4) and data types (minimum 4) • Support for 8/10/12/14/16-bit RAW data mode with capability of sign extension or zero padding to align with 16-bit memory addressing for RAW 10/12/14 modes • Support for user defined data types Please reference the MIPI CSI-2 D-PHY standard revision 1.2 for full receiver timing requirements. Please reference the AM273x TRM for a complete description of all programmable options.

    Check https://www.ti.com/product/AM2732 for details

    Best regards,

    Ming