Other Parts Discussed in Thread: OMAP-L138
I have an OMAP-L138 and an MSP430 communicating using their UARTs at 115,200 baud. The MSP430 is sending a 27-byte data packet every 13.5 milliseconds. While the MSP430 is sending data packets, I connect a USB HID device (I have tried a GPS and a mouse) and errors occur when parsing a couple of the data packets. An extra byte equal to 0 appears after the first byte of the packet and only the first 16 bytes of the packet are received. I have confirmed that the bytes are missing when they enter my application via a system read of /dev/ttyS1 (i.e. the errors are not a bug in my application). The same errors occur when I disconnect the USB device.
Any thoughts on what is going on? The UART has a 16-byte FIFO in hardware, which is enabled. Is a USB interrupt taking too long?
Any ideas on solutions? The hardware can't change, so I can't add HW flow control.
The OMAP-L138 is clocked at 300 MHz and is running the 2.6.33 Linux kernel (DaVinci PSP 02.20.00.12).
Thanks,
abkirchhoff